CANOPEN.SAMPLEPERIOD

Description

This parameter sets the fieldbus sample period (cyclic rate) which is the time between two PDO updates on the fieldbus cyclic channel. Use CANopen objects 60C2 subindex 1 (interpolation time period value) and 2 (interpolation time index) to adjust the CANOPEN.SAMPLEPERIOD over the fieldbus.

Formula:

SamplePeriod (seconds) = Interpolation_Time_Period_Value x 10^ Interpolation_Time_Index

For example, SamplePeriod = 1 x 10 -3 seconds, and this will set CANOPEN.SAMPLEPERIOD = 1000 microseconds. Kollmorgen recommends the following standard cycle rates, 250 µs, 500 µs, 1000 µs, 2000 µs, or 4000 µs.

Examples

Usage

For EtherCat:

The sample period must match the SYNC 0 period when using Distributed Clocks. The drive will not transition to OPERATIONAL mode when the SYNC 0 does not match the sample period.

Code

-->CANOPEN.SAMPLEPERIOD 2000
-->CANOPEN.SAMPLEPERIOD
-->2000 microseconds

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Microseconds

Range

250 to 1000 microseconds in increments of 250

1500 to 8000 microseconds in increments of 500

Default Value

2000

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CANOPEN.SAMPLEPERIOD

60c2h

01h

Unsigned8

-

-

Read/Write

No

CANOPEN.SAMPLEPERIOD

60c2h

02h

Signed8

-

-

Read/Write

No

CANOPEN.SAMPLEPERIOD

68c2h

01h

Unsigned8

-

-

Read/Write

No

CANOPEN.SAMPLEPERIOD

68c2h

02h

Signed8

-

-

Read/Write

No